If SDA/SCL pullup resister use 2.5kΩ, is it no problem?
・Datasheet rocommended 5kΩ resister.
・Customer using 2.5kΩ pullup. Sometimes, device's ACK isn't return.
⇒I think that pullup is one of the cause.
Best regards,
Satoshi
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
If SDA/SCL pullup resister use 2.5kΩ, is it no problem?
・Datasheet rocommended 5kΩ resister.
・Customer using 2.5kΩ pullup. Sometimes, device's ACK isn't return.
⇒I think that pullup is one of the cause.
Best regards,
Satoshi
Hi Satoshi,
From Datasheet Design Requirements section:
"The TMP102 device requires pullup resistors on the SCL, SDA, and ALERT pins. The recommended value for the pullup resistors is 5-kΩ. In some applications the pullup resistor can be lower or higher than 5 kΩ but must not exceed 3 mA of current on any of those pins."
Can you please verify the current do not exceed 3mA of current on any of those pins?
Mayrim