Hi,
I am working on the design of earbuds with sensors. I would like to get body's temperature and pulse from them. My first guess is to use an IR temperature sensor aiming at the ear drum and a PPG circuit aiming at the cavum conchae. The earbuds needs to be custom for each user so the sensor should fit inside of them (I could leave wires connected to another external circuit like a electronic necklace, using i2c for example). It should also be comfortable as people are suppose to sleep with them (So, an ear clip wouldn't be fine and the earbuds should not protrude out of the ear). Of course, power is also another key point in this design...
How good will be this device to be placed inside of an earbud and to get core body temperature? Do I have to aim it to the ear drum?
I will need to have audio there too. How could I fit both devices into the earbud without having issues?
Thanks.