I have read in the TMP007 datasheet
"Device Functional Modes (continued)
7.4.3 Nonvolatile Memory Description
7.4.3.1 Programming the Nonvolatile Memory
The TMP007 has an internal memory that can be programmed eight times."
(TMP007 Infrared Thermopile Sensor with Integrated Math Engine, SBOS685C –APRIL 2014–REVISED JULY 2015)
Is anyone able to tell me, why there are only 8 cycles for writing to the thermopile? Do i need to change the IC if i have already 8 wirte cycles?
If it is a flash memory, it does not make any sense.
Kind Regards,
Matthias