Hello,
we use the TMP122 AIDBVR since year 2003 and the Sensor Offset was always typically +/- 0,8 °C.
Since 2014 with LOT 2087108NFM and 4205224NFM we have a mean Offset of +1.47 °C and +1,57 °C. Maximum is +1.92 °C
Many Sensors are out of the Specification +/- 1.5 °C.
We measure the sensors on the PCB at Vcc= 5V on a metal plate in a chamber with 23 °C and 3 calibrated PT100 Sensors.
Can you send the Temperature Offset test data of these two Batches?
Can we return the Sensors of LOT 4205224NFM and get Sensors within Specification?
Thank you in advance