This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Web,
Your understanding is correct and the TMP007 address pins are provided precisely for this type of situations.
How are the address pins connected? Are they hard-wired or GPIO controlled? Please note that they need to be stable before communication starts.
If you continue to have problems, please forward a sketch of the wiring diagram and possibly a photo showing bus waveforms.
Regards,
Guang-Apps Sensing Products
Thank you very much.
I've verified my hard-wired connection with stable 3.3V/GND and found the same result that:
(ADR1, ADR0) = (1, 0) or (0, 0).setting can both get sensor data when SENSOR_I2C_ADDRESS defined in Sensor_tmp007.c is 0x44, while (0,0) cannot get data in 0x40.
I'll do another PCB soldering tomorrow to see if there is some wiring or layout bug. If the same condition exists, I'll simplify the sensorTag code first to narrow down to only TMP007 communication, and then update the SDA/SCL signal with my sketch.
Thank you again.
Best regards,
Webb
Excuse me. I think I still not get it thoroughly.
I'm a bit confused to map the A2 A1 A0 to the hard-wired ADR1 and ADR0.
If I connect (0, 0), then SMBus address 0x40, so (A2, A1, A0) = (0, 0, 0)?
From Figure 22 it seems reasonable. But how about Figure 23? The slave address bit 4 is 1, so read and write has different slave address?
The following figure is from my software setting 0x44 and hardware setting (0, 0).
What I think it is to read register 1: Local temperature, and I can see the data keep sending to my phone.
But it seems to be more like Figure 22 to read data.
Sorry I haven't successfully do another PCB yet.
But just from Figure 22, Figure 23, and Table 2 of the datasheet, I'm a bit confused about the slave address concept.
If any explanation or reference document would be grateful.
Best regards,
Webb
Hi Webb,
You are probably reading from a previous version of the data sheet. Please click on here: TMP007, it will bring you to the current data sheet.
Regards,
Guang-Apps Sensing Products