This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Does TI have a resistor set output temperature sensor?

Other Parts Discussed in Thread: TMP708, TMP709, LM57

I’m looking for a temperature device where I can attach a resistor to set when a particular temperature has been read.

As an example, if I attach a 10K resistor it will output a low when 65C is met or I could attach a 8.2K and the device will output at 62C. In other words a full temperature module in a SOT123, with an output that triggers at a certain temperature set by an external resistor.

I don’t need super accuracy – say +-2.5C.

Do we have anything like this?