On the TMP007, there is a register at address 0x10 called C2, which is used in calibration. However, none of the equation have a C2 coefficient in them. Equation 5 in the TMP007 Calibration Guide has a "C" coefficient.
Does the C2 Register control the C coefficient? Or something else?