Hello,
I am using TMP006B in my project on custom PCB
The measured temperature has huge offset of about +90 C°
I tried to adjust the calibration coefficients, but the only change the result by +-10 C°
Interestingly, if I set the Number of Averaged Samples (through control registers) to 1, the error is huge, like 800°C
The more samples i average, the close is my result to the real world. As if first one or two conversions are completely false.
The voltage to TMP is stable, although i dont have oscilloscope to measure it precisely.