I am currently evaluating a 4 sensor TMP107 system setup using a PIC18F microcontroller with a buffer connection to the 1st sensor as in section 8.2.1 (Figure 39. Connecting Multiple Devices) of the TMP107 document , SBOS716B -MAY 2015 - REVISED SEPTEMBER 2015 . The setup and processor are running off 3.3V.
In another TI document, the Application Report SBOA138A ( Easy-to-use Cabling Interface for Measuring Temperature with the TMP107). It is indicated in section 2.8 (page 8) that the resistor R3 (100 ohm) in Figure 6 (Examples USB Port-Based Control Board) is for ESD current limiting and glitch attenuation .
- Is the above mentioned ESD function similar to that in my setup mentioned earlier, and also will this be enough to protect against possible overvoltages?
- If not, any suggestions (e.g. diode based) for a suitable esd protection setup at the input (I/O1 - pin 3) of the 1st sensor in the daisy chain which will not affect the system performance?
Thanks