Hello E2E!
I have a customer who is interested in the TMP006.
Are there any curves available to show the accuracy/sensitivity of TMP006 around 41 degree C ? I didn't see anything in the datasheet.
Thanks!
Russell
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Russell,
My colleague is able to get a preliminary data for human body temperature range. I am not sure if you have looking for die temperature or object temperature, but below is the data that we collected for one device.
Coefficient calculated for Tobj = 36°C to 40°C, 55mm distance, 10 samples per point, 3.3V
Hope this helps!
Aaron
Hi Russell,
The temperature in blue is the die temperature, and the temperature in red is the target object temperature. The number inside the box are the temperature error. For example, if the object temperature 42°C, and the die temperature is 10°C then your temp error is 1.48°C.
Note: The data is collected only for one device.
Hope this clarify! Let me know if you have any question.
Aaron
Hi Aaron, to make this measurements did you change the FoV of the TMP006 like in https://www.youtube.com/watch?v=GEGiEi6tcVo ?? Also are this values the same (or at least very similar) for the TMP007?
thx in advance,
Federico.