I plan to use the LM34AC for sensing temperature in a wall mounted thermostat. The remote sensors will use the TO-92package, but I'm not sure how to best measure temperature in the wall mounted unit. I can put a hole in the case, stick the TO-92 through the case to the outside surface of the case, or stick it out a bit and epoxy it in place. However, this is a rather messy solution.
It occurred to me that if I used the SOIC package I could connect the unused pins to the thermostat case (with static protection) so the pins would transfer the temperature into the IC package and so to the sensor better than through the exposed part of the case of a TO-92.
Does anyone think this would work?