Hi,
We are now developing a body temperature sensor using TMP007, which measures the temperature on the eardrum. TMP007 is quite new to us, yet we have the expectation that it should response quickly since it is based on IR measurement.
However, what we observed from our prototype is a super slow response. Every time when we plugged our sensor into the ear, the direct reading of Tobj started from about -10°C. Then, it took about five minutes to reach a stable reading about 40°C.
We haven't done a calibration that can possibly adjust the final reading to a normal body temperature. All the configurations are default, while a full FOV is used.
What we now do not understand is:
1. Why is the response so slow?
2. Why does the measurement always start from a negative temperature?
We must admit that our PCB layout didn't strictly follow the guideline. Can it be the problem? We just designed a single layer PCB with very small size where the chip was placed. It is then connected to the main board using wires back on the PCB. The main board is placed far away from the sensor and does not have direct contact with it.
At last, we would like to post the measurement we got:
THX