Hi,
Customer is considering LM75B. Then, the device is assured t1,SCL Period (MIN)=2.5us. It is 400kHz(MAX) in other words.
If SCL clock has 50% duty, the low of t1≒1.25us for 400kHz. However, tlow is defined as 1.3us(min) as follows. I believe that the setting seems to violate I2C specification.
http://www.nxp.com/documents/user_manual/UM10204.pdf
Could the LM75B be used with SCL=400kHz(Duty=50%)?
Best Regards,
Kato