Hi,
My customer are designing LM96163 and facing an issue:
When reading the temperature via Remote Temperature Signed MSB (offset 0x1), the value is smaller than the actual one around 10 degrees centigrade deviation.
After setting RDTE (0x30) to 0, the issue seems improve. The default value of RDTE is 1.
Could you please help to confirm should they set the value to 0?
Please tell me what is this register purpose? Why change this bit can improve the issue?
Thanks