HI
Does LMT88DCKR have ESD MM spec?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Kevin,
As a policy TI no longer supports the machine model ESD specification on new devices, we instead support the charged device model (CDM) which more realistically represents what would happen to the device in a production environment.
The datasheet shows that the Charged-device model (CDM), per JEDEC specification JESD22-C101 rating is ±250 V.
Please note that the JEDEC document JEP157 states that 250-V CDM allows safe manufacturing with a standard ESD control process.
But I have found out that this is a mistake that this should be a machine model specification per JESD22-A115 at 250V. So you have your answer and we have a mistake that will be fixed at the next datasheet update. At that time we will also publish the CDM ESD rating as well.
Thank you and big apologies for the delayed response to your question.
Take care,
Hi Emmy,
so can i say that
1. after the TI policy, all of TI production do not provide this kind spec?
2. If customer still want to have it, can i say i can use CDM to replace MM spec?
3. Can you provide me the policy documentation?
thanks.