Part Number: TMP006EVM
Hi
I’m trying to log temperature data by using the sm-usb-dig module with a TMP006EVM module. The SW I’m using is also called TMP006EVM.
I have more than 5 devices of each which I have tried to get in contact with and even interchanged them with no luck.
I mostly get a failure “TMP006 did not ack” on almost all of them. One of the sensor does give data but it is incorrect. I have attached the log data from this sensor.
The data are recorded in normal ambient condition.
Most of the devices have been working before when I was running windows 7. Now we have upgraded to win 10 and it is not working anymore.
Is it because the driver is not compatible with windows 10? Have anyone else similar experience with windows 10 and this device + SW tool?
Please advice
br
Arun