This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMP708: Voltage on SET Pin

Part Number: TMP708

Hi everybody,

one of our customers uses the TMP708AIDBVR to detect an over temperature case at 105°C. He had some problems with the stability/precision.

He added a cap at the SET pin and everything was fine.. After that he removed the cap again and measured the voltage on the SET pin.. Attached you find the results (AC Coupled). There are high peaks on the voltage if he doesnt add the cap.. 

They think the peaks come from the PFC stage which is very close to the Pin/Resistor. But the question is how should the voltage look on the pin? It should be a stable DC voltage right? Or is there any intern circuit which could cause the peaks?

thanks

Bastian