This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM95071: Software driver compatibility between LM71 and LM95071 ?

Part Number: LM95071
Other Parts Discussed in Thread: LM71,

Hello,

Can you confirm if the LM71* and LM95071* devices are "100% compatible" at the software driver level?

I consider adding LM95071* as additional source to the LM71* that we currently use, and need to confirm interchangeability between the two in our 3.3V,SPI applications.

From what I read, only significant difference will be better accuracy from the LM95071.

Thank you!

Gilbert