Hi,
I'm looking for a remote temperature sensor that I can use in ATE, I need to monitor 9 thermal diodes (PNP).
Since the application is running in ATE, acquired temperatures need to be accessed at less than 10ms/channel.
I have an embedded controller that would access the remote thermal sensor device via I2C bus at speeds up to 1Mhz.
In the past, where I only needed to access up to 4 Tdiodes, there was plenty of time to acquire temperature, make a decision and then update the thermal solution.
But this new application where 9 Tdiodes on multiple chip module device will need to be assessed has me worried so I'm in search of a new remote sensor .
So my question:
Does TI have a multiple channel temperature sensor chip that would meet this requirement?
Thanks,
Sheldon Grooms
MTS AMD
512-779-6994