This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM35: Wrong reading at room temperature

Part Number: LM35

Hi,

We are using LM35 Temperature sensor on our boards but the sensor is attached to one of the sides of Heat Sink and not on the center. In some cases the LM 35 measures 220 - 250 mV at room temperature. However in most of the cases the reading is 356 or 321 mV at room temperature. Do you have any recommendation for using the part with Heat sink. Our heat sink is shared with 3 other parts and the pins of LM35 are soldered on board without touching any portion of Heat sink would it make any difference.

Please let us know.

Thanks,

Priyanka