Other Parts Discussed in Thread: CC1310
Tool/software: TI-RTOS
Hi
I have a question.
I used cc1310 to drive TMP112 acquisition temperature. When TMP112 in shut down mode, the current consumption is 2.2 uA, Data manual is 1 uA.
Why is this?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Ren
I weld an independent tmp112 module (onlyTMP112、 upper pull resistors and capacitors), The power and pin (SCL and SDA) are connected to the 3.3 V and IO ports on the MCU board. The multimeter current is connected to the positive electrode of tmp112. The measured current value was 2.2 uA
The connection diagram is shown below:
Ren Schackmann said:How are you measuring current consumption? Is there activity on the I2C bus during your measurement?
Ren
The connection diagram is shown below: