Part Number: TMP006EVM
Using the TMP007EasyCal, TMP006EVM_GUI, or calling tio32_Open() myself from a program causes the DLL window to flash briefly (open and close). Is there a way to prevent the window from opening and closing every time tio32_Open() is called? I need to be able to detect if the TMP006EVM is plugged in and the way I am doing it is polling once and a while using tio32_Open() and tio32_GetBoardCount and then checking the number of boards. The result is the DLL flashing every time I call tio32_Open to check if it is plugged in.