This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB3210: About SM-USB-DIG Platform user guide

Part Number: TUSB3210

Hi Sirs,

Sorry to bother you.

We'll refer SM-USB-DIG Platform user guide to design.

Some questions need confirm.

1. Page 5 fig 4 General-purpose I/O port P0 [0.7],P1 [0.7],P2[0.7] Net name is not clear enough. Could you help check it?

2. Page 6 fig 5 If we only use I2C and direct connect to LED. Should we need reserve SPI signal and LVC07A/2G07 ?

3. Page 6 fig 6. 

  • 3. Page 6 fig 6. Looks 1T45 is level shift and DIR control function. But actually we not sure why need this IC. Could you help explain it?  

    4. Page 7 fig 7. Looks R5/R6 the voltage is show 1.8v? But actually if 3.3/2 that is around 1.65. So there have tolerance on this output?

    5. Page 7 fig 8. Why need us Q1?? Should we need connect  R1/R11 33ohm?

    6. Page 8 fig 9. What is EEPROM 24LC64 address?

    7. Page 9 Fig 12 We not sure why need to use 1G32 function. Could you help to explain it?

    Many thanks for your reply

  • Hi Sirs,

    Sorry for push,

    Have any update on this case?

    Thanks!!

  • We use SM-USB-DIG in some of our EVM, but we do not provide support for the design of SM-USB-DIG itself. We do not support the use of SM-USB-DIG outside of TI EVM.

    Ren