Other Parts Discussed in Thread: TMP007,
Hi team,
The customer would like to use TMP006 or TMP007 to measure the copper wire temperature.
His application is as below:
The copper wire is on the aluminum plate. The temperature for the aluminum plate is about 80 degree C.
The diameter of the copper wire is 0.1mm. Now the customer needs only to measure the copper wire temperature.
The customer's measurement results is when the TMP006 or TMP007 device and the aluminum plate is 10cm apart,
the TMP006 or TMP007 device can still measure the aluminum plate temperature and ignore the copper wire temperature.
Is it possible to change the FOV, SO, A1 and other parameters to only measure the 0.1mm diameter copper wire temperature?
Best Wishes,
Mickey Zhang
Asia Customer Support Center
Texas Instruments