What is the spectral wavelength range of LMT70?
Is this sensor suitable for land surface temperature monitoring from a vehicle?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
What is the spectral wavelength range of LMT70?
Is this sensor suitable for land surface temperature monitoring from a vehicle?
Kanaya,
Please clarify your application context. What surface temperature are you trying to measure? e.g. PCB? We do not have data regarding spectral response of the device. What spectral environment are you operating in? What accuracy and footprint are you targeting?
-Kelvin
Roads and residential areas surface temperature. Is this instrument suitable? and by spectral range I meant about the wavelength range (e.g. 6-10 micrometer) which is sensed by this sensor.
I will need to know about the accuracy, thermal time constant, cost etc. requirements before recommending a specific sensor suited for your application.
If cost is not a concern I would recommend starting looking at our digital temperature sensors where the system accuracy is guaranteed.
Our IC temperature sensor senses temperature by measuring the change in the junction Vbe as function of temperature. This junction can be either on the same die (local) or external (remote). Temperature change is a function of heat transfer, which can include conduction, convection, and/or radiation. A more detailed explanation of this can be found here:
Accuracy should be within 0.5 deg.C. Is there any document available which gives information about spectral wavelength ranges of your sensors?