Hi
We have question of TMP431 functions.
1.
According to the datasheet, /ALERT can be de-asserted when the master reads the device address.
Is there any other condition that ALERT status is cleared?
2.
Is it possible to connect SCL/SDA to 3.3V and ALERT, THERM to V+ (5V)?
Even if that connection is accepted, is it possible to lead to degrade the accuracy of the measured temperature?
BestRegards