Other Parts Discussed in Thread: LM70
Dear All:
i use the LMT70 to measure the temperature , the precision is 0.1℃ at the 20 ℃--45℃, when i store the LMT70 to the -15℃ then take it out and place it at room temperature for one day to measure the temperature at the 20 ℃--45℃, i find the precision is only 0.15℃ at the 35-38℃ ,what cause the result? can you help to explain it? Thanks~