Hi team,
My customer use the LM20 in the power board in server.
The output of the LM20 is 1.4V. When they do the hot plug test of the power board, the output of the LM20 became the 2.7V and will keep 2.7V unless they power off the LM20.
And they found in the hot plug test, the 3.3V power for the LM20 has a vibration, see below.
The 3.3V power for the LM20 is the yellow one.
So can this vibration cause the problem?
How can we solve this problem?
The schematic is showed as below:
Please help to analyze this issue.
Lacey
Thanks a lot!