Other Parts Discussed in Thread: CC1310, LMT01
Hello, we are looking for a highly accurate (preferably as accurate as LMT70) and relatively cheap, SMD temperature sensor in order to apply it for the measurement of the cold water pipe surface temperature. Our initial idea was to use a SMD sensor that would have a contact with a pipe surface with its sensing side over a thermal pad whereas the other side would be soldered to the PCB that wouldn't have a direct contact with a pipe surface. Now when we discovered the LMT70 our understanding is that its recommended to sense the temperature over the PCB surface (through vias?) since the "balls" that are soldered to the PCB surface are more conductive than the other side of the LMT70. Did we understand that correct?
Given our application requirements, is LMT70 suitable for the pipe surface temperature measurement or could you please recommend any other sensor?
Thank you in advance.
Best,
Timur