Tool/software: Linux
We intend to use the TMP411E, which should be fully register and pin compatible with the ADT7461. Because of the SMB, there is a minimum SCL frequency of 1kHz, otherwise a timeout will be caused, which resets the device. When we set the two maximum temperature registers, we dont't intend to access the SMBus afterwards, so there will be no more SCL clock on the device. If we don't disable the timeout function, this will cause a reset condition. The question is now: does this exclusively reset the SMBus or does this reset affect the whole device including all registers like e.g. the maximum temperature regs? When only resetting the SMBus, this would be a great feature to prevent the device from "hanging" when a non finished frame had occoured.