Dear Technical Support Team,
I have a question about TDC7200 Caribration.
1.)
When CALIBRATION1 and CALIBRATION2 registers are updated?
Datasheet describes following. Are these mesured from "START" signal?
-------------
The first is a measurement of a single clock cycle period of the external clock.
the second measurement is for the number of external CLOCK periods set
by the CALIBRATION2_PERDIOS in the CONFIG2 register.
2.)
Is it possible that START_MEAS is "1" and CALIBRATION1/2 are updated at the same time.
I worry that CALIBRATION1/2 are reset before readout.
3.)
Are CALIBRATION1 and CALIBRATION2 updated while FORCE_CAL=0 except for interrupted measurement like counter overflow or missing STOP signal?
Dose it mean that caliblation is not perfomed only causing illegal situation?
4.)
What setting of CALIBRATION2_PERIOD is better for minimizing vary?
measuring 40CLOCK periods?
Best Regrds,
y.i