Part Number: TDC1000-GASEVM
Hello,
We are working on a gas flow meter with 200kHz transducers, and would like to use symmetrical excitation like described in SNAA284.
I am struggeling a bit with Figure 8, where in receive mode the transducers are connected with 2 x 10pF capacitors to GND.
R12 is 200R. The impedance of C3/C4 or C5/C6 should be much higher than R12, and when receiving, the transducers have no other connection to GND, how can that work? Would it not e required to connect the other end of the transducers to GND when in receiving mode?
Thanks, BR, Arne Sieber