Part Number: TDC1000-GASEVM
Hello. I am trying to get the TDC-1000-GASEVM to work. The problem seems to be in the configurations. When i connect it to the Oscilloscope i can see all the signals mentioned in the user guide, but i can't get the system to make sense. The system seems to generate TOF - measurement without having recived a stop signal. when i push air through the measuring device i get no response, always show zero flow. My transducers are 352 kHz, jumper is placed on CPU clock. Attached are screenshots of my configuration
Can someone help me figure out what is wrong in my configurations.