Dear all,
I am try to test how to measurement timing by tdc7200.
1. I am using default seting.
2. I using 1 GPIO from MCU to generate START signal to Pin 3, and delay around 10ms and generate STOP signal to Pin 4.
I hope that Interrupt signal at Pin 8 must go low but it do not. And I see that, I only go low when I read/write data of tdc7200 via SPI
Any idea how to test it?
p/s I am using 13Mhz at pin 5 and read/write data at register is correct now.
Thanks and regards