Part Number: TDC1000-GASEVM
I'm currently conducting an experiment to see how the TOF varies with O2 Concentration.
I have a TDC1000-GASEVM/TDC1000-BSTEVM and am using the TDC1000_7200_EVM Software.
However, the graphical output of the measured TOF is very noisy and fluctuating by about 100ns, when it should be quite constant if the O2 concentration is constant (i'm using a portable oxygen concentrator to provide flow through the sensor)
It also outputs a fluctuating TOF when the sensor isn't connected to any oxygen source.