Part Number: TDC1000-TDC7200EVM
I am having difficulty reading any form of data when I switch the settings of the firmware to Mode 2. I have attempted many different configurations of all the settings including the settings described in Bahram Mirshab's document (3603.Interfacing a water flow sensor to TDC1000...). I am able to capture data on the graph on the firmware and can save the data in the file when the firmware is set to Mode 0, but nothing when it is set to Mode 2 (I select start graph but no data shows on the graph and no data is saved to the file despite the PCB blinking as if it were reading data and the bottom of the firmware saying "Reading Graph Data Successfull"). I am using a different pipe than the one used in Bahram Mirshab's document, so I am not sure if that is the issue or if there is an issue with something else. I have included the link to the pipe I am using below.
Please help if you can!
http://www.audiowell.com/en/product-detail.aspx?id=264
-Abbigail