Other Parts Discussed in Thread: PGA460,
Hello everyone on this forum.
I have 2 questions regarding the PGA460:
1) Is the device operable only using the UART? In other words, are all the comm interfaces independent? This questions relies on the fact that when a burst & listem command ends (executed on the Data Monitor view of the GUI ) I see some activity on the IO pin.
I'm designing my custom application using the PGA460-Q1 and just wanted to confirm that the device is fully usable through the UART interface only (either sincronic or asincronic). I have limited space and only able to use the UART. What I've read so far tells me that this is posible, but I'm asking just in case I'm missing anything.
2) Related to the previous question. What are the minimum requirements regarding its comms interfaces for the PGA460?
3) The S-to_M DAta Bytes section of the GUI only shows 54 bytes when executing a "transducer echo data dump" command. Isn't this command supposed to output 128 bytes? Is this a bug on the GUI software?
Thank you :).
Cheers,