My customer is using TDC1000 for & have following observations:
RF1 |
CF2 |
||
1000 |
56 |
2843.4940855323 |
KHZ |
RF2 |
CF3 |
||
5000 |
56 |
568.6988171065 |
KHZ |
With above settings the second signal is spurious signal with peak voltage more than the actual signal and its frequency is ~500khz.
Peak voltage of the actual signal -- ~-880mv
After that the frequency band is changed as per below
RF1 |
CF2 |
||
2200 |
56 |
1292.4973116056 |
KHZ |
RF2 |
CF3 |
||
3300 |
56 |
861.6648744037 |
KHZ |
Even with above settings also same problem observed. And also the peal voltage of the actual signal is decreased.
Peak reduced to 560mv from 880mv
Freq of spurious signal ~520 Khz
1. Please suggest the band pas filter values / components to have a band of 850Khz to 1.25Mhz.
2. Is there any relation to echo peak voltage and filter band?
3. Please suggest the cable that should be used b/w sensor and the TDC1000, Min cable length reqd: 2.5meters