Other Parts Discussed in Thread: PGA460
Hello,
Our customer would like to use the device for detection range from 10cm to 8m.
In the datasheet P.106 there is the description that "The lower frequency range of 30 to 80 kHz is the default operating range for common automotive and consumer applications for a step resolution of 1 cm and typical range of 30 cm to 5m.".
Can we use PGA460-Q1 for this range?
If yes, could you please let me know the reference condition for detect this range?
Is this depend on transducer specification?
If the device has any function for expand detection range, please let me know.
Best Regards,
Ryuji