Part Number: TDC1000-TDC7200EVM
Hi,
I want to know, is there any limitation is there to change tdc1000 register settings.
My applicatoin is to measure liquid height in steel tank with two ultasonic sensors both at different location on bottom of tank for this i am planning to excite both one after another. Can some one suggest me best TDC1000 working mode. I am planning to use mode 0 and in firmware i will change channel after each excitation. I heared that in mode 2 auto swaping is there so no need for channel swaping in firmware but in mode2 we have to use combination of TX1/RX1 and TX2/RX2. Is it possible to use TX1/Rx2 and Tx2/Rx1 combination in mode 2. If not why?
thanks