Part Number: TDC1000-TDC7200EVM
Hello,
I just started to measure fluid levels in a metal tank using the TDC 1000 board by mounting the ultrasonic sensor at the bottom of the tank just as in "How to perform liquid level sensing through the bottom of a metal tank".
However I'd like to avoid gluing the sensor to the tank. I sometimes get signal using all sorts of coupling media but it seems to me that the coupling media between the tank and the sensor is really important and that it also highly depends on the sensor and frequency. Do you have any experience on the crucial factors like maybe thickness, consistency of the coupling media or the frequency that is used best?
Moreover I'm struggling with the timing register on the evaluation board. I need a maximum time of 3.4 ms to detect the highest liquid level. Is there a way to to slow down the clock of the timing register or at least i´hinder the board from cutting the signal after 1ms?
All the best,
Glenn