Hello,
I have got custom board made for tdc7200. Controller interface if STM32 with TDC7200.
1. Able to read/write internal register of TDC7200.
2. configuration set is CONFIG1 =0x03 , CONFIG2 =0x40 for TDC7200, INT_STATUS = 0x03,
3. start,stop and tof is generated from controller. TOF value from 10 uSec to 100 usec for testing.
able to get trigger logic from TDC7200 after send byte CONFIG1=0x03 for start measurement in MODE 2. And reading register value after 10usec without implementing INTB.