Hi,
i have some questions about the piezo transducers.
I have to use two piezo sensors (one as transmitter and the other one as a receiver) and i need a receiver circuit.
I have to use some piezos at different frequencies (from 40kHz to 1MHz) and i know that already exists a driver for the transmission of the ultrasonic wave (DRV2700EVM); the question is, does it exist a similar EVM for the receiver transducer which i can connect to arduino (for example)?
Thank you for your precious time!
Luigi