Part Number: TDC1000-GASEVM
Good morning,
i'm using TDC1000-GASEVM in order to evaluate the distance between two 220 kHz transducers.
I've read the user's guide but if i connect an oscilloscope to the START pins the signal is zero.
Even if i measure the signal on TX1 it is zero.
Can someone help me?
These are the setting:
And these are the connections:
Thank you.
Luigi