Hi Team,
Could you please Answer the following questions,
- If I chose the fixed-gain mode for medium-power (9.3.5.3.1) and choose, for example, the gain code 64, then what is the mitigation and the reinforcement?
- If I have chosen 63, then I have an attenuation of -8 + 63 x 0.125 = -0.125? How then is the reinforcement?
- If I chose fixed attenuation mode (9.4.5.5) (see Table 9.), then I can put a value of 0-64 (instead of 0-63) in the register ATTENUATION_x and then get the formula -8 + 64 x 0.125 = 0dB?
- Is there a precedence rule for gcode entries in the registers MANUAL_GAIN_DTGC / ATTENUATION_x?
- How can I set the minimum gain of + 6dB (Attenuation: -8dB, Gain + 14dB)?
- Electrical Characteristics: TGC Mode, page 13:
Channel-to-channel phase matching 15MHz signal: 11 degrees
Which phase difference do I have, e.g. at 600kHz?
Can one calculate the value over a Delay?
Thanks you in advance,
Needhu