Other Parts Discussed in Thread: ENERGIA, PGA460, PGA460-Q1
Dear TI,
I'm currently developing an obstacle detection prototype for an AGV. I have to use a ARM based microcontroller. If the prototype system is succesfull a dedicated PCB will be designed.
I want to use 4 BOOSTXL-PGA460 boards connected to the microcontroller on 4 separate uart channels. Can I use the code found in the software development guide and remove everything TCI, SPI and OWI related.in order for this to work I have to set the MEM_HOLD and MEM_CS HIGH and COM_PD and COM_SEL LOW? are there more settings needed to be able to use a two wire communication without a bus?
I plan on using the EVM package with the GUI for testing and find the needed settings and put those in the microcontroller program. Does this seem like a good plan, or did I overlook something?
kind regards,
Glenn