Hi,
I am working on MSP430FR6047 base water flow meter. I am using AudioWell 25mm brass flow tube.
I ran "USSLib_GUI_Demo" and loaded default USS parameters from GUI application.
I found that the reading are much less than actual flow.
Then I found valid meter constant range is 0 to 22742000 as set it to MAX possible i.e. (22742000)
But still I am getting reading 10 times less than actual.
and if I increase meter constant above the range to match reading with actual flow then it is causing higher variation at low flow.
also at zero flow , reading fluctuates in +/- 10 LPH