Part Number: TDC1000-TDC7200EVM
TDC1000-TDC7200EVM board,
I started to communicate via USB to a computer and use examples.
However, during the process of updating the software, the LED example was selected, which could not be connected with the computer at present (USB development process will not recognize the block development version, even if the update driver can not be used normally), would like to ask whether there is a way to restore, or Is updated back to the original state, thanks
Steps I have already done:
1. If you have followed the steps in the manual, but still cannot use it, LED D2 will still not light. (LED D4 is normally powered)
2.
Already read 6.1 Jumpers and 6.2 LED descriptions,
The current situation is
"If the LINK LED is OFF, check the physical connection to the PC then verify if the correct firmware
Has been downloaded if the jumpers have been connected correctly."
3. Suspected that the previous use of MSP430 USB Firmware Upgrade (BSL_USB_GUI.exe), using the "Blink LED Example" update results in the current connection condition, so the need to resolve Firmware reset, is there a relevant way? Thank you.
4. The current failure of the Firmware Upgrade causes the USB communication computer to not correctly identify the development board (see Chapter 7 upgrade for no significance).
Also refer to Chapter 6 or Chapter 7 for problems that cannot be solved
problem:
A failed firmware upgrade causes the USB communications computer to be incorrect.
Driver can be installed, but the board cannot be started normally.
What is needed now is how to restore or reprogram the software, so that the development version can be correctly identified and started.