Other Parts Discussed in Thread: UCC27531, , PGA460, TDC7200, TLV61046A
Hi,
i am using the TDC1011 with the UCC27531 to drive my transducer.( TDC1000-GASEVM)
I have a step up converter that generates 28V.
Everything works fine but i dont know if the Burst i am sending is enought to drive a 1kW transducer.
Do i need a transformer to boost my 28v to like 280V maybe?
How does a transducer power is measured P = u*i (1000W = 1000V * 1A) ?
OBs: The PGA460 has only 11m of object detection. I need at least 100 meters