Hello everyone,
I'm looking for an ultrasonic pulser, since I'm working on a parametric loudspeaker project. I liked the LM96550 and the LM96551. But I ran into a problem: the frequency range.
In the datasheet, on page 6, in the Analog Characteristics table, it specifies: Fout Output Frequency Range, RL = 100Ω, Min: 1 MHz, Max: 15 MHz.
- Why the imposition of the minimum of 1 MHz frequency of operation? Is it due to some internal component? Is it because of the power? Well, usually the one that can operate up to a certain frequency, can operate at less frequency.
The problem is that I need to use the push button with 40 kHz transducers.
- Could I use the LM96550 or the LM96551? Would it work with 40 kHz transducers?
Regards
Marcelo